Part Number: SN74LVC1G123
In addition to the forum article "SN74LVC1G123: Glitch-Free Power-Up Reset on Outputs"
e2e.ti.com/.../947998
we get an undesired output pulse at power-up.
Our design holds !A and B low. !CLR and VCC come up together. In this case no output pulse should be generated.
We have a VCC rise time (10% to 90%) of ~ 0,2ms (25V/s).
Now, sometimes the output generates an pulse when VCC is rising. !A and B is holding low.
When I increase the rise time for example to 350µs there is no undesired output pulse generation.
Is there a defined minimum ramp time for VCC-rise at power up for Glitch-Free Power-Up Reset?
Thanks!