This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

74lvc14A current sink exceeding recommended max, but below absolute maximum

Even though the recommended max sink current for the 74LVC14a is 24mA, can I sink more as long as I stay below the 50mA absolute max without damaging or degrading the IC? I need to sink about 40mA, periodically, for about 2 seconds of a 10sec cycle (20% duty cycle). I do not have the room to "double up" on devices to put 2 in parallel to achieve greater sinking capacity. I suspect the only issue in using the single device to sink more than the recommended current is that the guaranteed max. VOL will be greater than the 0.55V specified, but no damage will be caused to the device. In fact, based on the max output impedance specified at 24mA and 0.55V, the max Vol will be about 0.9V. Can do this without overstressing the device? Thank you, Jorge