Other Parts Discussed in Thread: SN74LVC1G17-Q1, SN74LVC2G08-Q1
Hello,
Kindly review the attached design using SN74LVC1G08QDRYRQ1
Thanks,
Melbin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Kindly review the attached design using SN74LVC1G08QDRYRQ1
Thanks,
Melbin
Hello,
We are working on a project with SN74LVC1G08QDRYRQ1 in it.
Kindly review the attached schematics and let me know the review comments.
Hi Melbin,
Thanks for the opportunity to review your schematics.
It looks like you're using one AND gate as a buffer (A tied high) and the other to AND the buffered output and the signal INH_ENA_ISO together.
The parts that I can see on the schematic are fine. You can get rid of R2623 and short pin 1 of U348 directly to V_CAN_VIO. You might consider swapping that AND gate to a Schmitt-trigger buffer, depending on the input signal characteristics at PMIC_SS2. If it's a relatively slow signal, a Schmitt-trigger buffer will prevent errouneous outputs and added power consumption. SN74LVC1G17-Q1 would be a good choice.
I can't see the signals at PMIC_SS2 or INH_ENA_ISO, so I don't know if they are good or not. I would recommend signals that are near the power rails (0V and 3.3V) for logic low and high, and transition quickly between those rails (max transition time of 33ns).
Additionally, I can't see the load at OUT_1. I would recommend a light load (15pF to 50pF) and up to 24mA current drive.
Hey Melbin,
To add to what Clemens mentioned, if this topology is needed then you could use a device like the SN74LVC2G08-Q1.
Melbin,
I noticed that you have already posted this. In an effort to consolidate posts on E2E, I have merged the threads.
Best,
Danny