Part Number: SN74AHCT1G14
Hi all,
for a PCB assembly, one element that I specified in the BOM is TI's 74AHCT1G14DBV. Now, the PCB assembly service is asking me my to specify the device more precisely. Basically, they are correct as it's not a fully specified manufacturer part number.
Looking at the datasheet, there are 4 variants of this device available according to the manufacturer part numbers:
a) There are parts with the additional suffix T and R that indicate package quantity (250 and 3000, respectively). That does not make any difference to me as the required quantity is well below both numbers.
b) There are parts with the additional prefix "SN". As I understand it, the only difference is the material finish options:
- 74* = NIPDAU
- SN74 = NIPDAU | SN
Does that make any difference regarding the soldering process?
All in all, I think adding anything to this part number would not be helpful and rather over-specify the device.
When I buy from a distributor, I usually pick the article that costs less. Here, it's SN74AHCT1G14DBVR which costs half as much as the other variants.
Does that make sense?