Part Number: TXB0304EVM
Other Parts Discussed in Thread: TXB0304,
Hallo,
I am working with TXB0304EVM to interface a sensor (logic 1.8V) with a Bluetooth controller (logic 3V). Even though the EVM board came with TXB0304, in which the OE pin has to be pulled low with resistor as mentioned in the data sheet.
" The only difference between TXB0304 and TXBN0304 is the OE signal being active high and active low respectively."
But I could only make the board function properly when the OE pin held high with a pullup resistor. Am I missing out something here? Or is it a problem due to a wrongly assembeleld IC?
I was not able to find such an issue in the forum. Please help.
Best regards,
Adarsh