Part Number: LSF0204
Other Parts Discussed in Thread: SN74AXC4T774
Hi team,
we met one problem on LSF0204 and i attached the schematic below:
P20PCMS_G1_M1_VA_SCH _ 24-LEVEL.pdf
U8----MUX;
U10----Level shift;
MUX 2A pin from NXP LS1020 SOC SPI interface-SCK
When MUX S=1 (3.3V), MUX 2A=2B2 to 3.3V SPI FLASH device; (2A=0V, 2B1=3.3V)
When MUX S=0 (0V), MUX 2A=2B1 to level shift device; (2A=0.7V 2B1=0.7V,level shift A2 pin=0.7V)
When remove mux device, and short mux 2A and 2B1, 2A=2B1=level shift A2 =0.7V
we need to access the SPI FLASH(1.8V system) for PCI SWITCH Software update by using LSF0204 for 3.3V to 1.8v level shift, but for now, since Vi Low=0.7V, we could not access 1.8V FLASH.
could you help and give us some insight on finding the root cause?
BR
Brandon