This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I've been having a hard time getting this one shot pulse to function the way I would like it to. Any chance there is a sample schematic that I could look at to help me get the logic down. I need to figure out what I'm pinning out wrong. Thanks!!!
Hi Michael,
The first page of the datasheet gives this info:
You can only use one of the input triggers per channel - so either the +TR or the -TR should be terminated as explained above.
Other than that, this is the complete schematic:
I could draw it up with +TR tied to Vss and one with a connected to the signal source, but I don't think that would be much help for you.
Can you share your schematic? What are you trying to accomplish? What trouble are you having?
It's 12V/22W so around 1.8A draw. I'm going to try the CSD13381F4 Mosfet its rated for 2.1A and 12V. Hopefully it will work out. Do you think that will work as a driver? I'd like to find a N-channel mosfet thats through hole instead of SMT. Thanks for your advice!
I was able to get the circuit working with a valve using a N-channel mosfet 2sk727. I'm going to convert this to a PCB now, Thanks for your advice.