I am working with a Stellaris LM3S9D96 and PAN1325 in our project, and Bluetooth refuses to initialize.
Stepping through InitializeBluetooth, the failure happens in BSC_Initialize(), for which I have no source code, and
it returns a value of -4, which looks to be BTPS_ERROR_HCI_INITIALIZATION_ERROR.
I'm using code derived from the standard DK-LM3S9D96 eval software.
I noticed that the eval kit we have uses a PAN1323, and the unmodified eval software for Bluetopia works just fine with that module.
Are there known compatibility issues between the two modules (1325 and 1323), or their components? If so, is there anything like a patch for software to take care of the issue?
Thanks,
Ron Sturtevant