Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN
Dear TI Team
I am working with the TMS570LS0714 PZ package and use the SCI2 RX (LIN) pin to only receive the data send by a sensor resp. the transceiver inbetween.
Each frame is send at a rate of 10kHz and is defined as 6 bytes (1 stop, 8 data bits, no parity):

Given that: The baudrate is 921600 bit/sec, 8 bit data words, 1 stop bit, no parity, frame transmitted at 10KHz. One frame has 6 bytes:
This means:
- The time to send one byte is (1/921600)*(8data+1 stop+1 start) = 10.85usec
- The time to send all six bytes is (1/921600)*(8data+1 stop+1 start)*6 = 65.1usec
- The idle state (waiting time at high level until next frame) is (1/10kHz) - 65.1usec = 35usec
You can see that after the six bytes are transmitted, the data stream is set to high (idle state) until the next frame is send.
My question is:
Is it possible to somehow trigger the buffer in such a way to start reading the data after the idle state is finished?
I use the following command to receive the data "sciReceive(scilinREG, 6, &sci_cmd[0]);" in "sciNotification"
I have currently the problem that
1. the data bytes are randomly stored in sci_cmd (for example byte 1 is stored in sci_cmd[3])
2. the idle state is stored in some cases in sci_cmd -> 1111 1111 (which should not be the case)
Would be nice to hear your opinion. Thank you!