Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UNIFLASH: TMS320F28388D Run Target After Program Load/Flash Operation did not work

Part Number: UNIFLASH
Other Parts Discussed in Thread: TMS320F28388D

Trying to program the flash using UNIFLASH and debug emulator then have CPU1 run the code.  

Under Program>C28xx_CPU1 I have checked "Run Actions > Run Target After Program Load/Flash Operation"

No Reset Action is set.

I select and "Load Image" successfully, but the target does not run.

Is this feature supposed to start the CPU1 target after programming?  

If not, any suggestions on how to start CPU1 target using UNIFLASH?

Thanks.

Other observations where target runs:

1. Disconnected Debug Emulator USB from Computer powers down isolated FTDI chip, then when it is plugged in again FTDI chip is powered and target starts to run.

2. Cycling power to entire board will start the target as well.

================ Details ===========================

UNIFILASH version: 6.3.0.3193

Board based on MCU063A Design using TMS320F28388D running @ 200MHz with 20MHz XTAL

Switch positions:

S1:A Position 1 = ON, JTAG Enabled

S1:A Position 2 = OFF, ISO UART disabled

S2 = Mode 3, GPIO-84/72 = 1/1 = Flash/USB Boot Mode

J1:A USB Emulation connected to Computer using XDS100v2 USB Debug Probe