Part Number: MCU-PLUS-SDK-AM243X
Hello, I am using the AM243X to communicate with EntherCAT and the Demo I sampled was ethercat_slave_beckhoff_ssc_demo。

- When I use the SSC tool to generate the configuration source file, the following issues occur:

- it required "ecat_appl_cnfg.h" for the configuration files.


Copy the generated files to ${SDK_INSTALL_PATH}/source/industrial_protocols/ethercat_slave/beckhoff_stack/stack_sources/.
- When I start CCS, run demo(ethercat_slave_beckhoff_ssc_demo),
Building file: "C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/coeappl.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -I"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/kernel/freertos/FreeRTOS-Kernel/include" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/kernel/freertos/portable/TI_ARM_CLANG/ARM_CR5F" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/kernel/freertos/config/am243x/r5f" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/industrial_protocols/ethercat_slave/beckhoff_stack/stack_sources" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/industrial_protocols/ethercat_slave/beckhoff_stack/stack_hal" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/examples/industrial_protocols/ethercat_slave_beckhoff_ssc_demo/" -DSOC_AM243X -DTIESC_APPLICATION=1 -D_DEBUG_=1 -gstrict-dwarf -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -Wno-self-assign -Wno-parentheses-equality -Wno-tautological-constant-out-of-range-compare -Wno-address-of-packed-member -Wno-tautological-pointer-compare -MMD -MP -MF"coeappl.d_raw" -MT"Src/coeappl.o" -I"C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Debug/syscfg" -o"Src/coeappl.o" "C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/coeappl.c"
subdir_rules.mk:16: recipe for target 'Src/coeappl.o' failed
In file included from C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/coeappl.c:98:
In file included from C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/ecatslv.h:35:
In file included from C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/tieschw.h:16:
C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/tiescbsp.h:17:10: fatal error: 'xdc/std.h' file not found
#include <xdc/std.h>
^~~~~~~~~~~
1 error generated.
gmake: *** [Src/coeappl.o] Error 1
Building file: "C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/ecatappl.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -I"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/kernel/freertos/FreeRTOS-Kernel/include" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/kernel/freertos/portable/TI_ARM_CLANG/ARM_CR5F" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/kernel/freertos/config/am243x/r5f" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/industrial_protocols/ethercat_slave/beckhoff_stack/stack_sources" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/source/industrial_protocols/ethercat_slave/beckhoff_stack/stack_hal" -I"C:/ti/mcu_plus_sdk_am243x_08_00_00_21/examples/industrial_protocols/ethercat_slave_beckhoff_ssc_demo/" -DSOC_AM243X -DTIESC_APPLICATION=1 -D_DEBUG_=1 -gstrict-dwarf -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -Wno-self-assign -Wno-parentheses-equality -Wno-tautological-constant-out-of-range-compare -Wno-address-of-packed-member -Wno-tautological-pointer-compare -MMD -MP -MF"ecatappl.d_raw" -MT"Src/ecatappl.o" -I"C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Debug/syscfg" -o"Src/ecatappl.o" "C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/ecatappl.c"
subdir_rules.mk:23: recipe for target 'Src/ecatappl.o' failed
In file included from C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/ecatappl.c:95:
In file included from C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/ecatslv.h:35:
In file included from C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/tieschw.h:16:
C:/workspace/ethercat_slave_beckhoff_ssc_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang/Src/tiescbsp.h:17:10: fatal error: 'xdc/std.h' file not found
#include <xdc/std.h>
^~~~~~~~~~~
1 error generated.
gmake: *** [Src/ecatappl.o] Error 1

It has a gmake file compilation error and a fatal error where the xdc/std.h file is missing.

So, can automatically generated source files from TI AM335X samples (Texas instruments incorporated) be applied to the AM243X?
No reference files found to migrate.
And, The source files automatically generated by SSC tool are missing 'appllnterface.h' and 'xdc/std.h'.