Part Number: TMS570LS0914
Hello,
i want to use the flashAPI F021 and i am using safeRTOS operation system.
I already added the flashAPI in the linker script and configure two data sections:
flashAPI : RUN_START( FLASHAPI_Start ) RUN_END( FLASHAPI_End )
{
*/library/extern/FlashAPI/Fapi_UserDefinedFunctions.c.obj (.text)
*/library/source/Hardware/flashIf/flashTMS.c.obj (.text)
--library = */library/extern/FlashAPI/F021_API_CortexR4_BE.lib (.text)
}load = FAPIFLASH, run = FAPIRAM, palign(0x1000), table(BINIT)
MEM_DATA_SEC_0 : START( MEM_DATA_SEC_0_Start ) END( MEM_DATA_SEC_0_End )
{
--library = */library/extern/FlashAPI/F021_API_CortexR4_BE.lib <
FlashStateMachine.ScaleFclk.obj
FlashStateMachine.SetActiveBank.obj > (.data)
} > RAM palign( 0x2000 )
The task in which I want to use the flashAPI runs in user mode.
Both memsections were configured as mpu sections according to Cortex-R4F techincal reference manual on page 125 and 126 (ARM DDI 0363G, ID041111; p.125-126/436).
MEM_DATA_SEC_0: AP bit value b011, XN bit value 1, TEX[2:0] value 0b000, C bit value 0 and B bit value 0
flashAPI : AP bit value b011, XN bit value 0, TEX[2:0] value 0b000, C bit value 0 and B bit value 0
If i try to debug the sw, the first instruction executed in the ram section caused a prefetch entry. The value of the fault status register is 0x0D. This value is an permission fault.
Function that causes the permission fault:
Fapi_StatusType Fapi_BlockErase(uint32_t Bank, uint32_t Erase_Start_Address, uint32_t Size_In_Bytes)
{
Fapi_StatusType error = Fapi_Status_Success;
uint8_t ucStartBank = 0;
uint8_t ucStartSector = 0;
uint8_t ucEndBank = 0;
uint32_t* eraseStartAddr0 = (uint32_t*)Erase_Start_Address;
uint32_t* eraseStartAddr = (uint32_t*)Erase_Start_Address;
uint32_t Erase_End_Address = Erase_Start_Address + Size_In_Bytes;
//Bestimme Startadresse des Sektors, welcher geloescht werden soll.
for(uint8_t i = 0; i < SECTOR_TABLE_SIZE; i++) // for (i = 0; i < NUMBEROFSECTORS - 1; i++) 23.02.2018 mkh
{
if(Erase_Start_Address == (uint32_t)(SectorTable[i].dwStartAddr))
{
ucStartBank = SectorTable[i].bankNumber;
ucStartSector = SectorTable[i].sectorNumber;
eraseStartAddr0 = SectorTable[i].dwStartAddr;
eraseStartAddr = SectorTable[i].dwStartAddr;
break;
}
}
//Bestimmt bank des Sektors, welcher geloescht werden soll.
for(uint8_t j = ucStartSector; j < SECTOR_TABLE_SIZE; j++)
{
if(Erase_End_Address < ((uint32_t)(SectorTable[j].dwStartAddr) + SectorTable[j].length))
{
ucEndBank = SectorTable[j].bankNumber;
break;
}
}
if(error == Fapi_Status_Success)
{
//F021_CPU0_REGISTER_ADDRESS is defined as 0xfff87000 in FMC.h
//Fapi_initializeAPI((Fapi_FmcRegistersType *)F021_CPU0_REGISTER_ADDRESS, freqInMHz); /*used for API Rev1.5*/
error = Fapi_initializeFlashBanks(HCLK_FREQ); /* used for API Rev2.01 */
}
for(uint8_t bk = ucStartBank; (bk < (ucEndBank + 1u)) && (error == Fapi_Status_Success); bk++)
{
uint8_t k;
uint32_t remaining;
error = Fapi_setActiveFlashBank((Fapi_FlashBankType)bk);
if(bk == 0u)
{
k = ucStartSector;
remaining = Size_In_Bytes;
}
else
{
k = 0u;
}
error = Fapi_enableMainBankSectors(0xFFFF); /* used for API 2.01*/
if(!WHILE_SAFE(FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady))
{
error = Fapi_Status_FsmBusy;
}
if(error == Fapi_Status_Success)
{
do
{
error = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector,
eraseStartAddr);
if(!WHILE_SAFE(FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy))
{
error = Fapi_Status_FsmBusy;
break;
}
if(!WHILE_SAFE(FAPI_GET_FSM_STATUS != Fapi_Status_Success))
{
error = Fapi_Status_FsmBusy;
break;
}
remaining -= SectorTable[k++].length;
if(k < SECTOR_TABLE_SIZE)
{
eraseStartAddr = SectorTable[k].dwStartAddr;
}
} while((remaining > 0u) && (k < SECTOR_TABLE_SIZE));
}
}
if(error == Fapi_Status_Success)
{
error = Flash_Erase_Check((uint32_t)eraseStartAddr0, Size_In_Bytes);
}
return error;
}
Disassembly from the instruction that causes the permission fault:

As you can see the instruction that caused the permission fault pushes registers onto the stack.
Register content:

The stack pointer is within the permissible range.
Task stack memory range from the map file:
address length
08003000 00001000 safetyTask.c.obj (.bss:safetybuffer_1)
Any ideas on how to solve this problem please?
Kind regards
Aron