Other Parts Discussed in Thread: UNIFLASH
I used MSP432E401YT REV B from Launchpad instead of MSP432E401Y as they were out of stock and I am having trouble factory resetting it.
The msp432_factory_reset is not available so I manually load the .GEL file from ccs_base > emulation > gel > msp432_factory_reset

Target Congif:

XDS110 USB debugger on another launchpad connected to MSP432E4YT REV B on custom board using:
- TDI, TDO, TCK, RST, 3.3 & GND
I keep seeing this error:
CS_DAP_0: Trouble Writing Register DP_RESET: (Error -1013 @ 0x2) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
MSP432_Factory_Reset() cannot be evaluated.
Target failed to write register DP_RESET
at DP_RESET=1 [msp432_factory_reset.gel:44]
at MSP432_Factory_Reset()
- Is the pinout of MSP432E401YT REV B even the same as of MSP432E401YTPDT?
- How can I try to factory reset my custom board so that I can run new firmware?
- I tried to factory reset because I am unable to program the controller over jtag, not sure why it works fine on the launchpad but not on my board
- I can flash the .out file with uniflash but the controller does not toggle gpio at all.