Part Number: TMS570LS3137
Other Parts Discussed in Thread: DP83640
Hello, I'm trying to send this struct via lwIP udp multicast. But as you see I see the output on wireshark like this.
void setHeader()
{
Sync.header.header[0]=0 ;
Sync.header.header[1]=0x2 ;
Sync.header.header[2]=0 ;
Sync.header.header[3]=0x2C ;
Sync.header.header[4]=0 ;
Sync.header.header[5]=0 ;
Sync.header.header[6]=0 ;
Sync.header.header[7]=0 ;
Sync.header.header[8]=0 ;
Sync.header.header[9]=0 ;
Sync.header.header[10]=0 ;
Sync.header.header[11]=0 ;
Sync.header.header[12]=0 ;
Sync.header.header[13]=0 ;
Sync.header.header[14]=0 ;
Sync.header.header[15]=0 ;
Sync.header.header[16]=0 ;
Sync.header.header[17]=0 ;
Sync.header.header[18]=0 ;
Sync.header.header[19]=0 ;
Sync.header.header[20]=0 ;
Sync.header.header[21]=0 ;
Sync.header.header[22]=0 ;
Sync.header.header[23]=0 ;
Sync.header.header[24]=0 ;
Sync.header.header[25]=0 ;
Sync.header.header[26]=0 ;
Sync.header.header[27]=0 ;
Sync.header.header[28]=0 ;
Sync.header.header[29]=1 ;
Sync.header.header[30]=0 ;
Sync.header.header[31]=1 ;
Sync.header.header[32]=0 ;
Sync.header.header[33]=0X7f ;
}

Send function is simple as this;
void udp_send()
{
struct pbuf* p_buffer;
p_buffer = pbuf_alloc(PBUF_TRANSPORT, tampon_boyut_u16, PBUF_RAM);
memcpy(p_buffer->payload, p_tampon_u8, tampon_boyut_u16);
err_t err = udp_sendto(Gl.pcb, p_buffer, &dest_ip, dest_port);
pbuf_free(p_buffer);
}
Payload length is correct. So only the data is getting corrupted. My main goal is send PTP-sync message with UDP.
And also another question of mine is I have TMS570LS31HDK.It has onboard DP83640 (1588 PHY) and as I said before I'm trying to send and get PTP messages between 2 HDK. So far i can get the internal clock's values via MDIO and attach them approciately to UDP payload. Should I send the data like this or do I have to use another method?
So any help will be appreciated.
Thanks in advance.