This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti,
Is there any demo application / example available on usage of F021 Flash library? Also, on F021 package, there are many different libraries available for example, F021 API CortexR4 LE Library, F021 API CortexR4 LE L2FMC Library and etc. which library to choose for RM48x?
Regards,
Monish P
Hi Monish,
The example of bootloader uses the F021 flash library to erase and program the flash. bl_flash.c is nice example for you:
//***************************************************************************** // // bl_flash.c : Flash programming functions used by the boot loader. // Author : QJ Wang. ang@ti.com // Date : 9-19-2012 // // Copyright (c) 2006-2011 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Texas Instruments (TI) is supplying this software for use solely and // exclusively on TI's microcontroller products. The software is owned by // TI and/or its suppliers, and is protected under applicable copyright // laws. You may not combine this software with "viral" open-source // software in order to form a larger program. // // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS. // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL // DAMAGES, FOR ANY REASON WHATSOEVER. // //***************************************************************************** #include "bl_config.h" #include "bl_flash.h" #include "F021_API/F021.h" #include "flash_defines.h" //***************************************************************************** // //! Returns the size of the ist sector size of the flash in bytes. //! //***************************************************************************** uint32_t BLInternalFlashFirstSectorSizeGet(void) { uint32_t firstSectorSize; firstSectorSize = (uint32_t)(flash_sector[0].start) + flash_sector[0].length; return (firstSectorSize); } //***************************************************************************** // //! Returns the size of the internal flash in bytes. //! //! This function returns the total number of bytes of internal flash in the //! current part. No adjustment is made for any sections reserved via //! options defined in bl_config.h. //! //! \return Returns the total number of bytes of internal flash. // //***************************************************************************** uint32_t BLInternalFlashSizeGet(void) { uint32_t flashSize; flashSize = (uint32_t)flash_sector[NUMBEROFSECTORS-1].start + flash_sector[NUMBEROFSECTORS-1].length; return (flashSize); } //***************************************************************************** // //! Checks whether a given start address is valid for a download. //! //! This function checks to determine whether the given address is a valid //! download image start address given the options defined in bl_config.h. //! //! \return Returns non-zero if the address is valid or 0 otherwise. // //***************************************************************************** uint32_t BLInternalFlashStartAddrCheck(uint32_t ulAddr, uint32_t ulImgSize) { uint32_t count=0, i; uint32_t ulWholeFlashSize; // // Determine the size of the flash available on the part in use. // ulWholeFlashSize = (uint32_t)flash_sector[NUMBEROFSECTORS-1].start + flash_sector[NUMBEROFSECTORS-1].length; /* 3MB */ /* The start address must be at the begining of the sector */ for (i = 0; i < NUMBEROFSECTORS-1; i++){ if (ulAddr == (uint32_t)(flash_sector[i].start)) { count++; } } if (count == 0){ #ifdef DEBUG_MSG_L3 //UART_putString(UART, "\r Application Address should be aligned with flash sector start address!\r"); #endif return(0); } // // Is the address we were passed a valid start address? We allow: // // 1. Address 0 if configured to update the boot loader. // 2. The start of the reserved block if parameter space is reserved (to // allow a download of the parameter block contents). // 3. The application start address specified in bl_config.h. // // The function fails if the address is not one of these, if the image // size is larger than the available space or if the address is not word // aligned. // if(( #ifdef ENABLE_BL_UPDATE (ulAddr != 0) && #endif (ulAddr != APP_START_ADDRESS)) || ((ulAddr + ulImgSize) > ulWholeFlashSize) || ((ulAddr & 3) != 0)) { #ifdef DEBUG_MSG_L3 //UART_putString(UART, "\r Flash address and size check failed!\r"); #endif return(0); } else { #ifdef DEBUG_MSG_L3 //UART_putString(UART, "\r Flash address and size check passed!\r"); #endif return(1); } } uint32_t Fapi_BlockErase( uint32_t Bank, uint32_t Flash_Start_Address, uint32_t Size_In_Bytes) { uint32_t status; uint32_t Freq_In_MHz; uint8_t i, j, bk, ucStartBank, ucStartSector, ucEndBank; uint32_t *eraseStartAddr0; uint32_t *eraseStartAddr; int remaining; uint32_t Flash_End_Address; ucStartBank = 0, i=0, ucStartSector = 0; ucEndBank = 0; eraseStartAddr0 = (uint32_t *)Flash_Start_Address; eraseStartAddr = (uint32_t *)Flash_Start_Address; Flash_End_Address = Flash_Start_Address + Size_In_Bytes; Freq_In_MHz = SYS_CLK_FREQ; for (i = 0; i < NUMBEROFSECTORS-1; i++){ if (Flash_Start_Address == (uint32_t)(flash_sector[i].start)) { ucStartBank = flash_sector[i].bankNumber; ucStartSector = flash_sector[i].sectorNumber; eraseStartAddr0 = flash_sector[i].start; eraseStartAddr = flash_sector[i].start; break; } } for (i = ucStartSector; i < NUMBEROFSECTORS-1; i++){ if (Flash_End_Address <= ((uint32_t)(flash_sector[i].start) + flash_sector[i].length)) { ucEndBank = flash_sector[i].bankNumber; break; } } //F021_CPU0_REGISTER_ADDRESS is defined as 0xfff87000 in FMC.h //Fapi_initializeAPI((Fapi_FmcRegistersType *)F021_CPU0_REGISTER_ADDRESS, Freq_In_MHz); /*used for API Rev1.5*/ Fapi_initializeFlashBanks(Freq_In_MHz); /* used for API Rev2.01 */ for (bk = ucStartBank; bk < ucEndBank+1; bk++){ Fapi_setActiveFlashBank((Fapi_FlashBankType)bk); if (bk == 0){ j = ucStartSector; remaining = Size_In_Bytes; }else{ j = 0; } Fapi_enableMainBankSectors(0xFFFF); /* used for API 2.01*/ // Fapi_enableMainBankSectors(0xFF); /* used for API 2.01*/ while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy ); do{ Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, eraseStartAddr); while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy ); while(FAPI_GET_FSM_STATUS != Fapi_Status_Success); // remaining -= flash_sector[j++].length; remaining -= flash_sector[(bk*15)+(j++)].length; eraseStartAddr = flash_sector[j].start; }while((remaining > 0) && ( j < flash_bank[bk].numOfSectors)); } status = Flash_Erase_Check((uint32_t)eraseStartAddr0, Size_In_Bytes); return (status); } //Bank here is not used. We calculate the bank in the function based on the Flash-Start-addr uint32_t Fapi_BlockProgram( uint32_t Bank, uint32_t Flash_Start_Address, uint32_t Data_Start_Address, uint32_t Size_In_Bytes) { register uint32_t src = Data_Start_Address; register uint32_t dst = Flash_Start_Address; register uint32_t bytes_remain = Size_In_Bytes; uint8_t i, ucBank; uint32_t status; uint32_t bytes; uint32_t Freq_In_MHz; Freq_In_MHz = SYS_CLK_FREQ; if (Size_In_Bytes < 16) bytes = Size_In_Bytes; else bytes = 16; for (i = 0; i < NUMBEROFSECTORS-1; i++){ if (Flash_Start_Address < (uint32_t)(flash_sector[i+1].start)) { ucBank = flash_sector[i].bankNumber; break; } } if(( Flash_Start_Address == APP_START_ADDRESS ) || ( ucBank == 1 )){ Fapi_initializeFlashBanks(Freq_In_MHz); /* used for API Rev2.01 */ Fapi_setActiveFlashBank((Fapi_FlashBankType)ucBank); Fapi_enableMainBankSectors(0xFF); /* used for API 2.01*/ while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy ); while( FAPI_GET_FSM_STATUS!= Fapi_Status_Success ); } while( bytes_remain > 0) { Fapi_issueProgrammingCommand((uint32_t *)dst, (uint8_t *)src, (uint32_t) bytes, 0, 0, Fapi_AutoEccGeneration); while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy ); while(FAPI_GET_FSM_STATUS!= Fapi_Status_Success); src += bytes; //Size_In_Bytes; dst += bytes; //Size_In_Bytes; bytes_remain -= bytes; //Size_In_Bytes; if ( bytes_remain < 16){ bytes = bytes_remain; } } #ifdef DEBUG_MSG_L3 //UART_putString(UART, "\r Programmed the flash: "); //UART_send32BitData(UART, Size_In_Bytes); //UART_putString(UART, " Bytes. \r "); #endif status = Flash_Program_Check(Flash_Start_Address, Data_Start_Address, Size_In_Bytes); return (status); } uint32_t Fapi_UpdateStatusProgram( uint32_t Bank, uint32_t Flash_Start_Address, uint32_t Data_Start_Address, uint32_t Size_In_Bytes) { register uint32_t src = Data_Start_Address; register uint32_t dst = Flash_Start_Address; uint32_t status; int bytes; uint32_t Freq_In_MHz; Freq_In_MHz = SYS_CLK_FREQ; if (Size_In_Bytes < 16) bytes = Size_In_Bytes; else bytes = 16; Fapi_initializeAPI((Fapi_FmcRegistersType *)F021_CPU0_REGISTER_ADDRESS, Freq_In_MHz); Fapi_setActiveFlashBank((Fapi_FlashBankType)Bank); #ifdef DEBUG_MSG_L2 //UART_putString(UART, "\r Programming The Update Status.... \r "); #endif Fapi_issueProgrammingCommand((uint32_t *)dst, (uint8_t *)src, (uint32_t) bytes, //8, 0, 0, Fapi_AutoEccGeneration); while( Fapi_checkFsmForReady() == Fapi_Status_FsmBusy ); status = Flash_Program_Check(Flash_Start_Address, Data_Start_Address, Size_In_Bytes); return (status); } uint32_t Flash_Program_Check(uint32_t Program_Start_Address, uint32_t Source_Start_Address, uint32_t No_Of_Bytes) { uint32_t error=0; register uint32_t *src1 = (uint32_t *) Source_Start_Address; register uint32_t *dst1 = (uint32_t *) Program_Start_Address; register uint32_t bytes = No_Of_Bytes; while(bytes > 0) { if(*dst1++ != *src1++) error = 1; bytes -= 0x4; } #ifdef DEBUG_MSG_L2 //UART_putString(UART, "\r Program Flash Errors: "); //UART_send32BitData(sciREG1, error); //UART_putString(UART, "\r "); #endif return(error); } uint32_t Flash_Erase_Check(uint32_t Start_Address, uint32_t Bytes) { uint32_t error=0; register uint32_t *dst1 = (uint32_t *) Start_Address; register uint32_t bytes = Bytes; while(bytes > 0) { if(*dst1++ != 0xFFFFFFFF){ error = 2; } bytes -= 0x4; } #ifdef DEBUG_MSG_L2 //UART_putString(UART, "\r Erase Flash Errors: "); //UART_send32BitData(sciREG1, error); //UART_putString(UART, "\r "); #endif return(error); } uint32_t Fapi_BlockRead( uint32_t Bank, uint32_t Flash_Start_Address, uint32_t Data_Start_Address, uint32_t Size_In_Bytes) { register uint32_t src = Data_Start_Address; register uint32_t dst = Flash_Start_Address; register uint32_t bytes_remain = Size_In_Bytes; uint32_t status =0; int bytes; uint32_t Freq_In_MHz; Freq_In_MHz = SYS_CLK_FREQ; if (Size_In_Bytes < 16) bytes = Size_In_Bytes; else bytes = 16; Fapi_initializeAPI((Fapi_FmcRegistersType *)F021_CPU0_REGISTER_ADDRESS, Freq_In_MHz); while( bytes_remain > 0) { Fapi_doMarginReadByByte((uint8_t *)src, (uint8_t *)dst, (uint32_t) bytes, //16 Fapi_NormalRead); src += bytes; //Size_In_Bytes; //0x10; dst += bytes; //Size_In_Bytes; //0x10; bytes_remain -= bytes; //Size_In_Bytes; //0x10; } return (status); }