Part Number: MSP432-DEBUGGERS
Hello friends,
I have the following problem, and I hope you can me help solve. I am trying to read the status of a pin in the MSP432P401R, after he made a data transmission (TX), the CS pin goes High, and when all data finish he change the state pin to Low. In the debug mode, a follow the state of pin, but I dont see any change. I wrote the following code the goal it has when the function are called one interruption is required.
int main(void){
DRDY_Work();
while(1){
while(!finish_flag);
MAP_GPIO_disableInterrupt( GPIO_PORT_P4, GPIO_PIN4);
finish_flag=0;
MAP_GPIO_clearInterruptFlag( GPIO_PORT_P4, GPIO_PIN4);
MAP_GPIO_enableInterrupt( GPIO_PORT_P4, GPIO_PIN4);
}
}
}
void DRDY_Work(void){
MAP_GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P4, GPIO_PIN4);
GPIO_interruptEdgeSelect(GPIO_PORT_P4,GPIO_PIN4, GPIO_HIGH_TO_LOW_TRANSITION);
MAP_GPIO_clearInterruptFlag(GPIO_PORT_P4, GPIO_PIN4);
MAP_GPIO_enableInterrupt(GPIO_PORT_P4, GPIO_PIN4);
MAP_Interrupt_enableInterrupt(INT_PORT4);
}
void PORT4_IRQHandler(void){
uint32_t status;
status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P4);
MAP_GPIO_clearInterruptFlag(GPIO_PORT_P4, status);
/* Toggling the output on the LED */
if(status & GPIO_PIN4){
finish_flag = 1;
}
}
Thanks in advance