Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: MSP432E401Y
Hi experts,
My customer is having the exact same problem as before with the MSP-EXP432E401Y that they are using.
Could you please let me know if there is a solution to this problem?
The problem is summarized in the original thread, but I get "Error -615" and cannot access the MSP432E401Y on the evaluation board. We've done the same checks that I did in the original thread, and the symptoms are exactly the same. Also, as per MEM#16 of the errata, I ran the unlock sequence twice, but could not recover.
I was able to check the most recent thread about a similar phenomenon, but it did not contain any solution.
URL:e2e.ti.com/.../msp-exp432e401y-error--615-when-debugging-with-msp-exp432e401y
The customer is still in the evaluation phase, but if you have any information on this issue, it would be appreciated if you could share it. There is no problem using private chat, etc.
Best regards,
O.H