Part Number: SM470R1B1M-HT
Hello,
I have a SM470R1B1M-SK evaluation kit and I am able to program in FLASH my application (and board examples) but I cannot program it in RAM.
I have used the evaluation board JTAG, J-LINK LITE IAR 091013 REV 8.0 and IAR V9.10.2 with a 14 day license (first day, not expired).
I also tried to program it with J-Link-ARM-KS (IAR JTAG) - also, worked for FLASH but not for RAM.
This is the error that I got:
Thu Oct 14, 2021 00:07:59: Warning: Failed to measure CPU clock frequency
Thu Oct 14, 2021 00:07:59: Could not detect CPU clock speed. Verification of test code downloaded into RAM failed.
I have read on this forum similar problems but without a clear solution.
My best guess is that the JTAG is limited and it cannot program the RAM, although it is more difficult to program the FLASH than the RAM.
For this microcontroller, SM470R1B1M-HT, the IAR is the only compiler/IDE that can program it without spending days to find a solution to program it - I have tried it and gave up.
Thanks,
Marius Raducanu