Part Number: TMS570LS3137
hi,When i call the function SL_SelfTest_SRAM(SRAM_ECC_ERROR_FORCING_2BIT,TRUE,&failInfoTCMRAM), the return value failInfoTCMRAM is ST_FAIL,but normal should be ST_PASS.
(1) I added the printing information in the function SL_SelfTest_SRAM(), and found that the condition in the red box in the figure below does not hold. That is to say, when the fault is injected into a 2bit ECC fault, only B1TCM has a fault flag bit, but B0TCM does not generate a fault flag bit. why?
(2) The parameter SRAM_ECC_ERROR_FORCING_2BIT is an ECC fault that generates 2BIT, but the parameter SRAM_ECC_2BIT_FAULT_INJECT is also generate 2 BIT ECC fault,What is the difference between the two before?