Part Number: TM4C123GH6PGE
Hello there
I asked my question on this topic before, but I think the topic has been locked because time has passed since the last message;
e2e.ti.com/.../tm4c123gh6pge-can-protocol-with-can0- base
The details are in the title I shared the link above, but to summarize briefly:
I cannot communicate with the CAN0 port on my custom board that I set up with TM4C123GH6PGE. But I can communicate with the same code from the CAN1 port.
As Charles said in his last message, I made the necessary modifications to the board and the PB4-PB5 pins and the simple_tx code still did not work. When I look with an oscilloscope, I can't see anything on the pins.
In case there is a problem on the board, I soldered the pins directly over the MCU to the can transceiver TX-RX pins with a cable. This did not change the result, still CAN is not working.
Could you please reopen the old topic so that the topic does not get messy? So I can move this message there.
Any help would be appreciated.