Part Number: MSP432E401Y
Hello,
Has anyone in the community performed or know if the MSP432 is capable of SPI functionality with an SD card (without any sort of adapter)? Reading through the technical reference manual, I see the MSP432 has both a QSSI that supports Freescale SPI or TI synchronous serial interfaces and the EPI can be used with external peripherals or memory. Was just wondering if one or other is preferred? I'm mainly hoping to store .txt or log files to the SD card through some form of SPI on the MSP432. I appreciate the help!
Best,
TM