Part Number: AM2432
Hi, I am planning to use AM2432 micro controller for my project. I have some queries about the controller interface
- Can all the 5 SPI controllers use independently at the same time?
- What is the maximum speed possible by CAN bus (not FD)?
- Does each single core cluster of Arm cortex-R5F can work with 800MHz
- Is there any turbo frequency available?
- How much can be the power consumption of each cores? can we shut off single core?
- How many Parallel interface can be connect to GPMC?
- How the communication between the two cores
- What is the application for Real time Programmable unit
- How many Gb Ethernet ports are available. I saw 2 Ethernet ports (under General connectivity) and 2xGMAC under industrial connectivity
- How this micro controller is different from AM64x series
Best Regards,
William