This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843: Hercules TMS570/RM Icc derating clarification

Part Number: RM57L843

In the datasheets for TMS570/RM series microcontrollers, the typical and maximum values for Icc are given at fgclk = 330 MHz.

There is a derating factor that the notes imply can be applied to the maximum value. However, they do not say they can also be applied to the typical value. Can someone please clarify if this derating can be applied to the typical value and if not, what derating can be applied?

Excerpt from RM57L843 datasheet: