This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I want to use two RTI notification compare. However, It only interrupts when the 'compare period 0' reaches the specified value (30000). The 'compare period 1' (1000) does not work.
Following, I attach the code of rtiNotification.
void rtiNotification(uint32 notification) { uint8_t i,j; uint16 A2 = 0x00, A1 = 0x00, A0 = 0x00; uint8 exTime0 = 0, exTime1 = 0; switch (notification) { case rtiNOTIFICATION_COMPARE0: /* enter user code between the USER CODE BEGIN and USER CODE END. */ /* Toggle HET pin 15 */ gioSetBit(hetPORT1, 15, 1); //0x00100000 gioSetBit(hetPORT1, 20, 1); //0x00100000 for(i = 0; i<10; i++){for(j = 0; j<10; j++){}} // It defines the pulse width gioSetBit(hetPORT1, 15, 0); //0x00000000 gioSetBit(hetPORT1, 20, 0); //0x00100000 break; case rtiNOTIFICATION_COMPARE1: exTime0++; if(255 < exTime0) { exTime0 = 0; exTime1++; writeCY15B(A2, A1, (A0+1), exTime1, 0, true); //Write in an external FRAM direction. } writeCY15B(A2, A1, A0, exTime0, 0, true); //Write in an external FRAM direction. } }
Thanks and regards,
Leandro