This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2431: Access from M4F in MCU domain to peripherals in MAIN domain

Part Number: AM2431

Hi,

My customer is now considering AM243x and some questions about M4F. Could you answer some their questions below ?

 

Can M4F on AM2431 execute the code on DDR4 ?

MCU domain is isolated from SoC on the Safety option F device, correct ?

On the safety-capable device (F option), M4F cannot access the peripherals in MAIN domain ?

MCU_CBASS0 interconnect in MCU domain is not connected to CBASS0 in MAIN domain on safety option device ?

 

Can M4F on AM2431 which doesn’t have F option access peripherals in MAIN domain such like DDR, PCIe, GPIO, etc… ? Can it access directly to the memory mapped registers of peripherals in MAIN domain ?

 

Are the both frequency of CBASS0 and MCU_CBASS0 250MHz ?  What are the bus width (bit) of CBASS0 and MCU_CBASS0 ?

  

Regards,

Hideaki