Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN, TMS570LC4357
Hi,
I am using the SPNA106D Application Report for initialization of the TMS570LS1227 controller and have queries regarding the following steps:
44. Verify that the dual-clock-comparator (DCC) module can actually detect and flag a frequency error
Would this involve setting the Counter0, Counter1 and Valid0 values so that the following error conditions are generated:
a. Counter1 counts down to 0 before Counter0 reaches 0
b. Counter1 does not reach 0 even when Counter0 and Valid0 have both reached 0
47. Run a background check on entire Flash using CRC and DMA
My understanding is this requires a CRC check on the entire Flash memory. Could you please clarify if this is correct and what role the DMA has here?
51. Set up the MPU for the bus masters
54. Configure desired access permissions for peripherals using the Peripheral Central Resource (PCR) controller registers
The Safety Manual states the API Name as "Not Applicable" with the Remark "Feature in Hardware". Does this mean that the above initialization steps are not applicable for the controller?
Would appreciate your help in this regard.
Thanks and Regards,
Vimal