This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: Long time to wake up from hibernate

Part Number: MSP432E401Y

Hi, 

Using the example from TI example code but adjusted to our application 

simplelink_msp432e4_sdk_4_20_00_12\examples\nortos\MSP_EXP432E401Y\driverlib\hibernate_vdd3on_rtcwake

It is configured to wake up every 4 seconds and rtc used to match. Has anyone measured how long time it takes for the MCU to wake up from hibernation. I am using a test pin to put high after the device wakes up every 4 sec. The only stuff done before the pin is set to high are: configuring the system clock to 48MHz, configuring a three ports and a few pins. Measuring with the oscilloscope it takes 20 ms after the pin HIB_N (pin 65) is high and before the test pin is set high. 

Regards,

Gergana