Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Hello
I am trying to set up an interrupt triggered by mcu_gpio0_8 in the main domain.
The setup is done like this:
rmIrqReq.valid_params = 0U;
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_ID_VALID;
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID;
rmIrqReq.global_event = 0U;
rmIrqReq.src_id = TISCI_DEV_MCU_GPIO0;
rmIrqReq.src_index = TISCI_BANK_SRC_IDX_BASE_MCU_GPIO0 + GPIO_GET_BANK_INDEX(SPI0_DRDY_PIN);
rmIrqReq.dst_id = TISCI_DEV_R5FSS0_CORE0;
rmIrqReq.dst_host_irq = ADC_DRV_DRDY_GPIO_INTR_NUM;
rmIrqReq.ia_id = 0U;
rmIrqReq.vint = 0U;
rmIrqReq.vint_status_bit_index = 0U;
rmIrqReq.secondary_host = TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST;
retVal = Sciclient_rmIrqSet(&rmIrqReq, &rmIrqResp, SystemP_WAIT_FOREVER);
This setup fails in Sciclient_rmProgramInterruptRoute()
Is there a way to do this?
Thanks