Hi,
I want to use wkup gpio0 interrupt in main domain, and how to config interrupt router ?


WKUP_GPIOMUX_INTRTR0_OUTP is not connected directly to the R5FSS0/1 but to R5FSS0/1_INTRTR0, and R5FSS0/1_INTRTR0 are connected to R5FSS0/1.
How to configure interrupt routes by Sciclient_rmIrqSet in this case ?
I try config as follow but it failed
rmIrqReq.secondary_host = TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST;
rmIrqReq.src_id = TISCI_DEV_WKUP_GPIO0;
rmIrqReq.src_index = 0;
/* Set the destination interrupt */
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_ID_VALID;
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID;
/* Set the destination based on the core */
rmIrqReq.dst_id = TISCI_DEV_R5FSS0_INTROUTER0;
rmIrqReq.dst_host_irq = CSLR_R5FSS0_INTROUTER0_IN_WKUP_GPIOMUX_INTRTR0_OUTP_30;
Sciclient_rmIrqSetRaw(&rmIrqReq, &rmIrqResp, SCICLIENT_SERVICE_WAIT_FOREVER);
rmIrqReq.secondary_host = TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST;
rmIrqReq.src_id = src_id;
rmIrqReq.src_index = src_index; /* This is the event coming out of the peripheral */
/* Set the destination interrupt */
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_ID_VALID;
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID;
/* Set the destination based on the core */
rmIrqReq.dst_id = TISCI_DEV_R5FSS0_CORE0;
rmIrqReq.dst_host_irq = CSLR_R5FSS0_CORE0_INTR_R5FSS0_INTROUTER0_OUTL_173;
Sciclient_rmIrqSetRaw(&rmIrqReq, &rmIrqResp, SCICLIENT_SERVICE_WAIT_FOREVER);
Thanks
Alex