This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I am using flash Api V2.01.0 of TI for TMS570LS1227. I am sharing with you my codes snip that fall the infinite loop. I saw two different mistake at code. When I push directly “Play” button at Debug Mode, code is run into Fapi_BlockErase function(at F_Api_2.PNG) and code goes to infinite loop at line 201(Picture BlockEraseFuntion) but when i paused the debug, it fall prefetch abort page. However if I use it with “StepOver” button step by step I can pass the BlockErase function and code can erease the flash banks after that it run into infinite loop at line 439 Fapi_Issue_ProgrammingCommand function (Picture F_Api_1) at debug mode. Then I stopped the code and saw my two byte data on flash memory at debug mode.
Also I am using three different disable Interrupt functions ( _disable_interrupt_() / _disable_IRQ_interrupt_() / _disable_FIQ_interrupt_() ) before go in to fapi functions.
Can you offer different things about this and do you have flash programming code example for TMS570LS1227 ?
Hi Onur,
Are the F021 Flash APIs and related code/constants copied to RAM, and executed from SRAM?
The API related code is bl_flash.c in your example. You can use this way to map the section to RAM, then copy this section to SRAM in your main():
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI:
{
.\source\Fapi_UserDefinedFunctions.obj (.text, .data)
.\source\bl_flash.obj (.text, .data)
--library= "c:\ti\Hercules\F021 Flash API\02.01.01\F021_API_CortexR4_BE.lib" (.text, .data)
} palign=8 load = FLASH0, run = SRAM, LOAD_START(apiLoadStart), RUN_START(apiRunStart), SIZE(apiLoadSize)