Part Number: TMS570LS0914
Hey TI,
We configured the dma-packet as frame transfer with Element Count = 4 and Frame Count = 10.
If we are connected with a debugger, it seems that the values from our destination buffer are updated only if the reg_dma->CFTCOUNT reaches zero.
We thought, that the values shall be updated every time when there is a new frame.
1) Why are the values updadated so late?
2) Where does the dma module cache the values?
3) If we stop the appication with a breakpoint, does the DMA modul run in the backround?
4) If we set a breakpoint, is it possible that values from the destination buffer are overwritten?
Best regards,
Thorben