Part Number: TMDXRM46HDK
Other Parts Discussed in Thread: UNIFLASH
I have been trying to get my CCS IDE to work with the Hercules Safety MCU Dev Kit RM4 MCU. In the beginning the demo would run, I selected the pre set led.
I could not compile the code above after I compiled it. It said it failed to verify, much like a previous post. Using CCS 11.1.0
I would like to get Project 0 and CAB Bus bootloader examples to compile and flash onto the board.
Now after trying a few things the board does not run the leds in a pattern when power is applied and the IDE and uniflash utility
I tried no longer sees the xds debug probe on the board. It looks like I may have lost the boot or something on the board or the
code for the debug probe.
What can I do to get the dev board back alive. Then I can address compiling the code.
Paul Hembrook
Presco Inc.