This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I want to bring up FreeRTOS FAT file system (fs/freertos/fat) on the FreeRTOS -- not nortos. But current SDK source code supports nortos only.
Do you have plans to support FreeRTOS?
I modified makefile.am243x.r5f.ti-arm-clang to support FreeRTOS.
I removed source/fs/freertos_fat/portable/nortos/portable.c and removed source/fs/freertos_fat/portable/nortos include path.
I added ff_locking.c and ff_time.c file in the FILES_common. I added FreeRTOS include path.
When I tried to build the library, I got a compile error as below:
Compiling: freertos_fat.am243x.r5f.ti-arm-clang.debug.lib: C:/ti/mcu_plus_sdk_am243x_08_03_00_18/source/fs/freertos_fat/FreeRTOS-FAT/ff_stdio.c
In file included from C:/ti/mcu_plus_sdk_am243x_08_03_00_18/source/fs/freertos_fat/FreeRTOS-FAT/ff_stdio.c:34:
C:/ti/mcu_plus_sdk_am243x_08_03_00_18/source/fs/freertos_fat/FreeRTOS-FAT/include\ff_stdio.h:155:10: error: Please define space for 3 entries
#error Please define space for 3 entries
^
1 error generated.
Here is compile error code in the ff_stdio.h:
#if ( ( configNUM_THREAD_LOCAL_STORAGE_POINTERS - ffconfigCWD_THREAD_LOCAL_INDEX ) < 3 )
#error Please define space for 3 entries
#endif
Both values are defined as below:
#define configNUM_THREAD_LOCAL_STORAGE_POINTERS (4) <- FreeRTOSConfig.h
#define ffconfigCWD_THREAD_LOCAL_INDEX (4U) <- FreeRTOSFATConfig.h
Do you have any suggestions for this issue?
Hi Chaehee,
The configNUM_THREAD_LOCAL_STORAGE_POINTERS is set as 4 for general use cases. We have not yet added support for FreeRTOS_FAT with freertos. The steps used by you are correct for porting. Corrections you need to do it configNUM_THREAD_LOCAL_STORAGE_POINTERS to be increased to 6 as FreeRTOS_FAT itself uses 2 threads. Also you might need to increase the heap in your linker file to support configNUM_THREAD_LOCAL_STORAGE_POINTERS as 6.
I see the definitions of portINLINE are present for M4/A53 core but not for R5F core. I will raise a ticket for the same. Thanks for pointing this out.
Thanks and Regards,
Aakash