This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: How to use the SDXC card 64 or 128GB instead of SDHC card 32GB for High volume capacity.

Part Number: TMS570LC4357


Hi QJ Wang,

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1095921/tms570lc4357-how-to-use-the-sdxc-card-64-or-128gb-instead-of-sdhc-card-32gb-for-high-volume-capacity

Santhosh: 

How to use the SDXC card 64 or 128GB  instead of SDHC card  32GB for High volume capacity. 

QJ Wang : 

TMS570 doesn't have a dedicated native SDCard interface. You can use SPI to interface with a SD Card if this SD card supports SPI mode.

 I haven't tried a SDXC card on TMS570 HDK. I think it should work if it supports SPI mode.

Can you share me any support reference code for SDXC card code related to TMS570 HDK ?

 

  • Hi Santhosh,

    Both SDHC and SDXC support SPI mode. They use the same SPI protocol. 

    SD card: Capacities range from 128MB to 2GB,

                   Format: FAT16

                   SD cards will work in all host devices that support SD, SDHC, or SDXC

    SDHC card:  Based on the SDA 2.0 specification.

                         Capacities range from 4GB to 32GB

                         File Format: FAT32

    SDXC card: Based on the SDA 3.0 specification

                        Capacities range from 64GB to 2TB

                        Filet Format: exFAT

    Because SDXC uses a different file system called exFAT and it works differently than standard SD cards and SDHC cards. We don't have example to reading and writing fro/to SDXC cards.

  • HI QJ Wang,

    Can you share the library for SDXC card read and write which is used in any other MCU other than TMS570 .

    Share me the link which TI MCU is used this library for SDXC ?

    Thanks in advance.

    Santhosh

  • Hi Santhosh,

    As I said, we don't have example of SDXC SD card.