Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: SYSCONFIG
Dear Community,
after switching to the SDK Release 08.04.00.17 we are facing the issue, that the option for selecting the "Number of Data Lines" is no longer available.
In the SDK 08.03.00.18 this option was available (see attached screenshot.
SDK 08.03.00.18, Sysconfig 1.12.1:

SDK 08.04.00.17, Sysconfig 1.13.0: --> The option is missing, there are eight datalines predefined.

When I open the example for the launchpad, there are only four data lines (--> QSPI), when I open an EVM example, there are eight data lines (--> OSPI).
How can we change this option?
As we are using QSPI on our custom board this selection is mandatory for us.
We are also required to switch to the SDK 08.04.00.17 because of the HS FS feature of the new chip revision (Rev. B).
Thanks in advance for you support.
Best Regards
Robin