Part Number: LAUNCHXL2-570LC43
Other Parts Discussed in Thread: TMS570LC4357
Hello
I am trying to run Launchpad/570LS/570LC43/Project_0 from the source tree obtained from https://git.ti.com/git/hercules_examples/hercules_examples.git
It is not working, I get into an undef state right from the reset. System details: Ubuntu 22.04LTS running on a 64 bit PC, CCS 11.1.0.00011 , target LAUNCHXL2-570LC43
By disassembling the code at/near address 0, I have some idea why it is not working; it seems that the binary code is junk.
Below is the output from the disassembly window (the _c_int00 symbol is at 0x21CC and has valid code in it)
Also note that I have not modified anything in the source tree.
What could I be doing wrong?
52 b _c_int00
$../source/HL_sys_intvecs.asm:52:66$(), resetEntry():
00000000: 710800EA smlattvc r8, r10, r0, r0
54 b undefEntry
undefEntry:
00000004: FEFFFFEA cdp2 p15, #0xf, c15, c15, c10, #7
56 b svcEntry
svcEntry:
00000008: FEFFFFEA cdp2 p15, #0xf, c15, c15, c10, #7
58 b prefetchEntry
prefetchEntry:
0000000c: FEFFFFEA cdp2 p15, #0xf, c15, c15, c10, #7
60 b dataEntry
dataEntry:
00000010: FEFFFFEA cdp2 p15, #0xf, c15, c15, c10, #7
61 b phantomInterrupt