Part Number: AM2431
Other Parts Discussed in Thread: TDA4VM, SYSCONFIG
Hi,
I'd like to check which Flash protocol are supported by the OSPI interface of AM2431 among 1) Hyperbus/Infineon, 2) Octabus/MXIC, 3) Xccela/Micron. Are they all supported. Do you have a specific register setting for each protocol to specify which Flash is connected to the SoC?
Page2: "1× Flash Subsystem (FSS) that can be configured as one Octal SPI (OSPI) or one Quad SPI (QSPI) flash interface"
Thanks
Alex