Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: AM263x peripheral clock configuration using sysconfig

Part Number: AM2634
Other Parts Discussed in Thread: SYSCONFIG

Hi TI Experts,

I am using MCUPlusSDK version 8.3.1.05, with SYSCONFIG 1.12.1 but in sysconfig didn't found a option to modify the core Clock , SYSCLK and other peripheral clocks.

currently in the example projects i can see by default the clock is configured as 400MHz coreclock and 200MHz SYSClock.

any suggestion how to configure/modify the clock.

Regards

Bikash

  • Hi TI Team,

    Can you please help me with this topic, I am interested to know how to modify the clock configuration with MCUPLUSSDK.

  • Hi Bikash, 

    Currently the clock configuration is GEL based. Upon connecting to the R5 the gel will execute "Configure_Plls_R5F_400_SYS_200_Clocks()," which calls multiple funciton to achieve an R5 clock of 400MHz and a sysclk of 200MHz. 

    In the OnTargetConnect() script we have:

    ...
    
            //Configure PLLs
            Configure_Plls_R5F_400_SYS_200_Clocks();
    
            //Enable all peripheral clocks
            Configure_All_Peripheral_Clks();
        }else{
            GEL_TextOut("Warning !! None of the scripts executed in this mode\n");
        }
    }

    Where "Configure_Plls_R5F_400_SYS_200_Clocks()" calls for "Program_Core_PLL()" located in "AM263x_PLL.gel":

    hotmenu Configure_Plls_R5F_400_SYS_200_Clocks()
    {
        if(Enable_OnTarget_Connect == 1){
            Program_Core_PLL();
            Program_Per_PLL();
            Program_SYS_CLK_DIVBY2();
            // Switch R5SS and SYS_CLK to Core PLL, so that R5 run at 400MHz
            Program_R5F_SYS_CLK_SRC();
            GEL_TextOut("\n CLK Programmed R5F=400MHz and SYS_CLK=200MHz \n");
        }else{
            GEL_TextOut("Errrrr... Please Load Gel files\n");
        }
    }

    hotmenu Program_Core_PLL() 
    {
        unsigned int val_pll_core_stat = 0;
        unsigned int val_pll_per_stat = 0;
        unsigned int val_hsdiv_clkout;   
    
        val_pll_core_stat = Read_MMR(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_STATUS);
        if((val_pll_core_stat & 0x00000400) != 0x00000400)
        {
            // N
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_M2NDIV, 9, 8, 0);
            //M2
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_M2NDIV, 1, 7, 16);
            
            //M
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_MN2DIV, 0x320, 12, 0); 
           
            //N2
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_MN2DIV, 0x0, 4, 16); 
    
            //SD divider of the PLL with the value of 0x8 to get the optimum jitter performance
            Write_MMR_Field(0x53200418, 8, 8,24);
            
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_CLKCTRL, 0,1, 23);        //Idle
    
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_CLKCTRL, 0,1,0);  		//Soft Reset
    
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_TENABLE, 1,1,0);          // PLL_CORE_TENABLE = 1;
            
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_CLKCTRL, 1,1,0);          //Soft Reset
            
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_TENABLE, 0,1,0);          // PLL_CORE_TENABLE = 0;
                
            Write_MMR(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_TENABLEDIV, 1);                 // PLL_CORE_TENABLEDIV = 1;
            Write_MMR(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_TENABLEDIV, 0);                 // PLL_CORE_TENABLEDIV = 0;
            
            do
            {     
                val_pll_core_stat = Read_MMR(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_STATUS);
            }while( ((val_pll_core_stat & 0x00000400) != 0x00000400) ) ;
            
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_HSDIVIDER_CLKOUT0, 0x4, 5, 0);//CLKOUT0
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_HSDIVIDER_CLKOUT1, 0x3, 5, 0);//CLKOUT1
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_HSDIVIDER_CLKOUT2, 0x4, 5, 0);//CLKOUT2
            
            
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_HSDIVIDER, 1,1,2);   // PLL_CORE_HSDIV_TENABLEDIV = 1;
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_HSDIVIDER, 0,1,2);   // PLL_CORE_HSDIV_TENABLEDIV = 0;
            
            
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_HSDIVIDER_CLKOUT0, 0x1, 1, 8);//CLKOUT0
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_HSDIVIDER_CLKOUT1, 0x1, 1, 8);//CLKOUT1
            Write_MMR_Field(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_PLL_CORE_HSDIVIDER_CLKOUT2, 0x1, 1, 8);//CLKOUT1
            
            GEL_TextOut("CORE PLL Configuration Complete \n");
        
        }
    }

    You can use this script as an example by modifying the M and N dividers as well as the HSDIVIDER values to output the desired values for the output clocks.

    Details on the variables used for configuring the PLLs can be found in section 6.4.1.2 Analog Modulesof the TRM. Also, for more detailed instructions on how to configure the Core PLL please refer to section 6.4.1.2.3.1.2 Sequence to Configure the CORE PLL

    Best,

    Daniel

    Link to the TRM: AM263x SitaraTm Microcontroller Technical Reference Manual (Rev. B) (ti.com)

  • Thank you Daniel for the details.