Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN,
Hello, thank you for always answering my questions.
Today, we ask about the block size problem of FEE Virtual Sector.
I want to set the Number of Virtual Sector to 2 to store a total of 64 Kbyte data divided into blocks. However, when the Flash Start Sector of Virtual Sector1 is set to 0 and the Flash End Sector is set to 1, and the Flash Start Sector of Virtual Sector2 is set to 2 and the Flash End Sector is set to 3 and the block size is set, the sum of the FEE block sizes is 32Kbyte at the maximum.
Virtual Sector1 and 2 are each 32Kbytes for a total of 64Kbytes, but I don't know why the block size cannot be set above 32Kbytes.
FEE Virtual Sector Configuration says "Please make sure that all Virtual Sectors are configured to be of the same size", "Please make sure that Virtual Sectors do not overlap".
However, when I set Flash Start Sector of Virtual Sector1 to 0, Flash End Sector to 3, and Flash Start Sector of Virtual Sector2 to 3 and Flash End Sector to 3, I set the sum of the FEE block sizes up to 64Kbytes.

Will there be any problems using FEE with the above settings?
Thank you for your time. Have a nice day