Part Number: AM2432
Dear TI Experts,
I managed to create a HS Device using the OTP Keywriter.
The dummy keys were used during this process, so from my understanding I should be able to run a hs_fs image on my board without additional steps.
I also tried to adapt the "deviceconfig.mak" script in the SDK by selecting "HS" device. This caused the build process to produce a tiimage marked with "hs" instead of "hs_fs".
Should I use this file?
Here is the parsed socid information that I receive from the ROM BL:
-----------------------SoC ID Header Info:-----------------------NumBlocks : 2-----------------------SoC ID Public ROM Info:-----------------------SubBlockId : 1SubBlockSize : 26DeviceName : am64xDeviceType : HSSEDMSC ROM Version : [0, 2, 0, 0]R5 ROM Version : [0, 2, 0, 0]-----------------------SoC ID Secure ROM Info:-----------------------Sec SubBlockId : 2Sec SubBlockSize : 166Sec Prime : 0Sec Key Revision : 1Sec Key Count : 2Sec TI MPK Hash : b018658ad99dc903c8c9bfb27b12751099920a042ad1dfea7b7ba57369f15546de285edde6a7b39a8bdc40a27b237f8fb1e57f245e80b929c1e28b024aa2ecc6Sec Cust MPK Hash : 1f6002b07cd9b0b7c47d9ca8d1aae57b8e8784a12f636b2b760d7d98a18f189760dfd0f23e2b0cb10ec7edc7c6edac3d9bdfefe0eddc3fff7fe9ad875195527dSec Unique ID : c4c73513e945cce9469cf3ef891b36852b3233b1574a6b30a71cf988efa2bb93
Thanks in advance for your support.
Best Regards
Robin