Part Number: TM4C1290NCPDT
Hello
we have a system with 35 boards with the above ARM.
once a day or so the board connected to ethernet loses communication, I understand it falls into FaultISR, when debugging I actually saw that after days of waiting.
when going over the registers I went to the address of where the interrupt happened and this is what I saw:

the " branch FaultISR " is totally not understood because that is not the code I have there when I look into the files.
I understood that the problem happens in the DHCP timer interrupt when rechecking the IP although the IP cannot change as it is a standalone system
with a microtick dealing with the IPs - THAT DO NOT CHANGE.
Why do I see this branch to FaultISR?
Is this problem known from somewhere else?
What I did when reaching this fault is to save in flash the registers add 2 to the pc like in the TI example and leave - it works fine (when it happened - twice)
is this solution OK?
Maccabi