Part Number: MCU-PLUS-SDK-AM263X
Other Parts Discussed in Thread: SYSCONFIG
Hi,
May I know:
1, May I know if I can select anyone instance if I used only core0?
2, What is the map of intr_num with instance since I'd like ti register ISR?
in this example,
GPIO Pins in AM263x:
AM263x has 139 GPIO pins
The device has four instances of the GPIO module, one dedicated per R5FSS processor core
- Pinmux/IOMUX allows assignment of GPO pin control to a specific R5FSS processor core using a 4:1 MUX (MCUSDK sysconfig generates code automatically for configuring this)
- GPI pins are observable by all processor cores
The GPIO modules are capable of supporting a maximum of 144 dedicated pins. AM263x implements 139 pins.
GPIO Interrupts in AM263x:
Regarding interrupts,
From the GPIO modules, 180 events/interrupts reach as input to GPIO Interrupt XBAR as shown in diagram below.
The 180 inputs contain both the individual GPIO interrupts (144 muxed from 4 GPIO modules) and also the 9 bank interrupts of 4 GPIO module
| Number of Interrupts | |
| Single GPIO Pin Interrupts | 144 |
| GPIO Bank Interrupts for instance 0 | 9 |
| GPIO Bank Interrupts for instance 1 | 9 |
| GPIO Bank Interrupts for instance 2 | 9 |
| GPIO Bank Interrupts for instance 3 | 9 |
| Total Interrupts | 180 |

In the Current SDK 8.5 we have gpio_input_interrupt example using GPIO bank interrupt.
In the example Go to SysCfg --> GPIO INT XBAR Option.

To use the Individual GPIO Interrupt, change the XBAR Output option to respective GPIO_MUX pin required for you. Here ignore the "_MUX" in this context, this refers to the individual GPIO Pin only.

While acknowledging and checking the interrupt status for Individual and Bank GPIO Interrupts these APIs can be used:
| GPIO Bank | Individual GPIOs |
| GPIO_getBankIntrStatus | GPIO_getIntrStatus |
| GPIO_clearBankIntrStatus | GPIO_clearIntrStatus |