Part Number: TM4C129ENCZAD
When the USB is connected to the board on which TM4C129ENCZAD is mounted, the PC will look like the image below.

Just to confirm, when I asked the question last time, it was TM4C129ENCZAD
bootloader and firmware using JTAG
There was a flash.
Is there any problem with writing to TM4C129ENCZAD with this image?

Is there a way to confirm that the XDS110 debug probe and TM4C129ENCZAD are connected via JTAG?
I read the user guide, but I didn't understand it well, so I would like to know if there is a way.