Part Number: TMDSEMU110-U
Hi Team,
First, I was supplying power from a computer via a USB connection.
I wonder if TMDSEMU110-U can work as XDS110 debugger
Run the command from a command prompt to see if was typing.
Commands were entered from the following hierarchy.
C:\ti\ccs_base\common\uscif\xds110
The command is following:
(The reason is to check if it is possible to switch between DFU mode and Runtime Mode.)
xdsdfu.exe �Cm
After confirming that it was in DFU mode, I unplugged the power.
After turning the power back on again, the device is disappear from device manager.
Best Regards,
Tom