Part Number: AM2431
Hi Team,
1)
in table 7-17. page 145 of AM2431 DS there is stated CL should be between 6 and 12 pF.

Is this CL the external capacitors ( CL=CL1 = CL2)? or is this the load capacitance from quarz datasheet? or is this CL =
?
2) Second question regarding the calculation of CL (Cload)
in DS of AM2431 the following equation is used 
while in lot of other documentation including SNLA290 the following equation is used 
if we use CXI = 1.44pF , CXO = 1.52pF, Cpin = CXI+ CXO = 2.96pF
and CpcbXI = 1pF , CpcbXO = 1pf, Cstray = CpcbXI + CpcbXO = 2pF
and use CL1 = CL2 = 10pF
with first equation we get from AM2341 Ds we get CL = 6.24pF, and with second equation we get 9.96pF the difference is 3.72pF
Which equation is more accurate?
Because if i select crystal eg 10pF https://www.raltron.com/webproducts/specs/CRYSTAL/RH100-25.000-10-F-3030-TR-NS2.pdf
with first equation i have to use 18pf external capacitors and with second equation i have to use 10pF external capacitors
Best Regards,
d.





or should i add to CLA also the CpcbXO + CXO?