Hi,
Q: Is it possible to use for example ADC0_Ain0 for both the ADC0 and the comparator submodule at the same time? I do not know the internals about the analog signal routing. My intention is to digitize a motor current available on the input ADC0_AIN0 by the ADC and at the same time configure the comparator submodule to check for an overcurrent condition using the same input signal.
br
Markus