Part Number: MSP432E411Y
Other Parts Discussed in Thread: MSP-EXP432E401Y,
Hi,
Continuation of the post below.
After programming boot_uart_flash_MSP-EXP432E401Y.txt using a ROM-based bootloader, I get the following error:

I saw the waveform when BSL-Scripter.exe was executed on the command prompt above, but some data is sent from the microcomputer to BSL Rocket like BSL Rocket → MSP432 (yellow), then MSP432 → BSL Rocket (green) seems to be returning.

I am currently using the MSP432E411Y, so do I need a program for the E411Y? The C:\ti\BSL-Scripter\ScriptExampleWindows\E4xx_uart folder had only E401Y. If I need the txt file for MSP432E411Y, can you tell me how to generate it?
Thanks,
Eevee