Part Number: AM2634
The AM2634 shows the General Purpose Memory controller with an option of 16-bit parallel data bus (22-b address) under media and storage.
- Does that mean that code cannot be executed from this parallel port?
- Is correct to assume that code can be executed from QSPI and if so,
- at what speed?
- When transferring code from external flash to RAM on the fly, are other portions of the code still able to run?
- Do we have any metrics that compare speed of execution of RAM when multiple transfers are made from flash?
Thank you!