Part Number: TM4C123GH6PM
Hi Everyone,
I would like to sample some signals with a higher sampling rate than the effective sampling rate of the two ADCs (e.g., instead of 1 MHz maximum sampling, I would like to sample at 1.5-3 MHz). I know of the possibility of sample phase control, but as I have more than one signal, I don't think I can use it.
According to this topic on Stackoverflow it is possible to use multiple channels of an ADC to raise the effective sampling rate over the maximum sampling rate of the given ADC, if the ADC sequences through the channels.
My question is, is there some possibility to "go over" the 1 MSPS (1 MHz) sampling rate of this ADC, if so, which settings of the ADCs on this uC allow this (except the use of the sample phase control)?
Thank you for your answers in advance,
Best regards,
Zsolt