Other Parts Discussed in Thread: ADC1173
Hi fellows
I have a question.
Fist of all I am a chemist and I am working on one project, I need a fast and simultaneous measurements on tiva c series launchpad, at least I think so.
So this is the project: I would like to make a Frequency-Domain Lifetime
Measurements for long lifetime fluorophores. Anyway, I will have a two sin waves incoming with same frequency but one is shifted in phase compared do another, I am trying to read both of them simultaneously so after I can calculate phase shift and from that the lifetime of fluorescence of fluorophore.
I am wondering how much samples per second is posible to measure with Tiva™ C Series TM4C123G LaunchPad?
and is there somebody who knows, and is willing to post the code for reading of two inputs simultaneously, i need to read only one second of incoming data, I need a sampling speed up to 15MHz, Is that possible?
I have added simulation of sine waves so you have a clear view of what am I trying to do.